7/1/2013 6:41 AM | |
Joined: 1/28/2009 Last visit: 5/20/2024 Posts: 6840 Rating: (1359)
|
Hello, What kind of network ?PROFIBUS,ETHERNET or MODBUS? For 2 first cases, check the "s7 connection" between each selected partner. see the sample for 2 partners: How do you simulate communication between two CPU modules? Best regards Hamid Hosseini |
Last edited by: hdhosseini at: 7/1/2013 6:49 AM |
|
This contribution was helpful to3 thankful Users |
7/1/2013 6:50 AM | |
Joined: 5/28/2008 Last visit: 5/23/2024 Posts: 4506 Rating: (836)
|
Hello, It can be used for two CPUs or more.
|
Ayman Elotaify |
|
This contribution was helpful to3 thankful Users |
7/1/2013 7:05 AM | |
Joined: 11/8/2011 Last visit: 4/12/2024 Posts: 387 Rating: (43) |
HI profibus communication network in between 3 PLC315-2dp |
7/1/2013 7:53 AM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181) |
All of them are Masters? If they are - you can not make "real simulation"! |
7/1/2013 8:34 AM | |
Posts: 153 Rating: (2) |
Check these links also, you may find some thing useful to you...:: /tf/WW/en/Posts/92117 http://support.automation.siemens.com/WW/view/en/36068796 https://support.automation.siemens.com/WW/llisapi.dll/csfetch/36068796/S7_PLCSIM_V54_SP3.zip |
7/1/2013 9:07 AM | |
Joined: 3/18/2008 Last visit: 12/8/2023 Posts: 1750 Rating: (270) |
Hello, you cannot perform 100% error free software Test with Step7 PLC Sim all the time. Please have a look at similar FAQ which describes Limitation/Function not Supported by PLCSIM. Which components are not supported by S7-PLCSIM V5.4 SP4? Hope this helps. |
VANDE MATARAM..... |
|
This contribution was helpful to2 thankful Users |
7/3/2013 10:29 AM | |
Posts: 559 Rating: (87) |
This is really helpful. I was also searching for the same type of simulation solution between 2 plcs. Now I got it. Thanks to all
|
7/3/2013 10:39 AM | |
Posts: 559 Rating: (87) |
I also want to know one thing. Is it possible to communicate simulation software with hardware plc? Means communication between actual plc & plcsim software.
|
7/3/2013 11:08 AM | |
Posts: 559 Rating: (87) |
Dear Ayman This is the case if I want to simulate communication between 2 plcs & I have only one plc. Then can I use plcsim as 2nd plc?
|
7/3/2013 2:07 PM | |
Joined: 3/18/2008 Last visit: 12/8/2023 Posts: 1750 Rating: (270) |
Hello Soultionfinder, I have worked with some similar product called Simba Profibus available in siemens for simulation Purpose in PCS7. In my Project I communicated 4 AS with around six RIO(ET200M) in each AS. it is used to communicate Remote I/O's with S7 PLC using its own dedicated simba pro Software. With the use of that we can have a benifit in Saving of investments for test, commissioning and training systems. The Details information can be found here regarding the same. |
Last edited by: Amit_86 at: 7/3/2013 2:08 PMLast edited by: Amit_86 at: 7/3/2013 2:08 PMVANDE MATARAM..... |
|
This contribution was helpful to1 thankful Users |
7/4/2013 1:30 PM | |
Joined: 11/8/2011 Last visit: 4/12/2024 Posts: 387 Rating: (43) |
thanks for all reply i am getting error while simulating Please find the attached file |
Follow us on