2/22/2018 8:09 AM | |
Posts: 3 Rating: (0) |
Also 0ma = 50 Degrees Celcius 20ma = 0 Degrees Celcius |
2/27/2018 10:34 AM | |
Joined: 10/11/2006 Last visit: 7/26/2024 Posts: 5880 Rating: (798)
|
Hello callumpage I assume that a kind of ventilator speed shall be control the temperature. I would propose using the drives internal PID controller according to this example : https://support.industry.siemens.com/cs/ww/en/view/109483275 Turning the direction of the drive only I propose by p1820, which turns the phase output. Then the min. and max. frequency containing positively |
With best regards, |
|
Follow us on