12/7/2023 12:05 PM | |
Joined: 10/11/2006 Last visit: 7/2/2024 Posts: 5871 Rating:
|
Hello PISCEAN 2010, to configure a DCM with the option board CBE20 a Advanced CUD is necessary. How to configure the Profinet Communication is described in the operating manual of the DCM. Please find the manual under the following link: https://support.industry.siemens.com/cs/us/en/view/109825291 In chapter 10.5.1 the configuration is shown with the Starter software. To implement a DCM 6RA80 in TIA-Portal for Profinet communication please use the hardware catalog. You can find the CBE20 under the path: Other field devices / Profinet IO / Siemens AG / Sinamics / Sinamics DCM CBE20 V1.5 |
Last edited by: The Helping Hand at: 12/07/2023 12:35:55Link optimized With best regards, |
|
This contribution was helpful to
1 thankful Users |
12/13/2023 9:01 AM | |
Joined: 10/11/2006 Last visit: 7/2/2024 Posts: 5871 Rating:
|
Hello PISCEAN 2010, please find the link of the FAQ "How to add a SINAMICS DCM in the TIA Portal project as a PROFIBUS/PROFINET device?" under the following link: https://support.industry.siemens.com/cs/us/en/view/109783817 |
Last edited by: The Helping Hand at: 12/13/2023 09:21:50Link optimized With best regards, |
|
This contribution was helpful to
1 thankful Users |
Follow us on