3/11/2022 9:42 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating:
|
Hello Gopinathan, Please check alarm value in r2124, interpret it in hexadecimal & contact your Siemens support center. You can get detail troubleshooting of the alarm. Hope this helps. |
3/15/2022 8:21 AM | |
Joined: 7/13/2011 Last visit: 6/5/2024 Posts: 37 Rating:
|
Hello, Please find the attached Photos, which include Fault values of F1039. 1. First when visited RTG crane, Drive in factory reset condition.And this DCM drive have memory card also. 2. So i try to download original project backup to the drive.In my project i used DCC chart for some function. So i need to download first TPdcblib_SINAMICS_4_5.3.0 Library to drive. But why i try to download this library , can not possible to download and make library download error. 3. So i just did factory reset of drive, then just try RAM to ROM option. And immediately it makes F1039 fault. 4. Then i realized ROM memory was broken, after only i replaced new CUD board. Note : I have attched Uploaded project backup(when problem time), for NVM memory check. Thanks and regards Gopinath AttachmentFault Values and Uploaded backup(for NVM check).zip (496 Downloads) |
Last edited by: Gopinathan at: 03/15/2022 08:39:27 |
|
3/15/2022 10:10 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating:
|
Could not open attached back up file. Message pops up as program is write-protected. |
3/16/2022 8:55 AM | |
Joined: 7/13/2011 Last visit: 6/5/2024 Posts: 37 Rating:
|
|
3/16/2022 8:56 AM | |
Joined: 7/13/2011 Last visit: 6/5/2024 Posts: 37 Rating:
|
|
3/16/2022 8:56 AM | |
Joined: 7/13/2011 Last visit: 6/5/2024 Posts: 37 Rating:
|
AttachmentRTG201_Upload(Trolly Drive is OK).zip (426 Downloads) |
Follow us on