8/7/2019 9:04 AM | |
Posts: 153 Rating: (7) |
Thank you Can you check my program. Please suggest correction if any AttachmentRTG1_2.zip (362 Downloads) |
8/7/2019 10:58 AM | |
Posts: 153 Rating: (7) |
Hello standstill detection P1226 can not find in drive and CU both. Drive is using with hardwired hoist and gantry selection and do not use PLC communication. Drive ON/OFF1 and operation enable command is coming through hard wire. This program is working program which is created in Simotion V5.2. i have attached again with V4.5. AttachmentRTG1_Final.zip (372 Downloads) |
Last edited by: Soni. at: 08/07/2019 11:00:35 |
|
8/7/2019 11:09 AM | |
Posts: 153 Rating: (7) |
Please See the DCC pdf program i used AttachmentDCC_1.pdf (503 Downloads) |
Follow us on