Industry Online Support
Technical Forum
5/21/2012 5:58 PM | |
Posts: 767 Rating:
|
Hello Mothilal, The following part number would be for use with DRIVE-CLiQ ports within an enclosure. 6SL3066-4CA00-0AA0 SINAMICS/SINUMERIK/SIMOTION DUSTCOVER FOR DRIVE-CLIQ PORT SET WITH 50 PIECES The following part number would be external devices (i.e. outside of an enclosure): 6SL3066-4CA01-0AA0 SINAMICS DUSTCOVER IP67 FOR DRIVE-CLIQ PORT SET WITH 6 PIECES These items are documented in Siemens Catalog PM21 2011for selection. Unfortunately I do not see available a picture example of the internal version. Attached is scan pdf of catalog page showing as part of picture the external dust cover (IP67 protection rating). Deputy AttachmentDust Proof Blanking Plugs.pdf (490 Downloads) |
This contribution was helpful to
1 thankful Users |
Follow us on