2/28/2017 7:25 PM | |
Posts: 4 Rating: (0) |
Thanks a lot... Today I have been able to run the drive from both BOP-2 & from HMI/PLC using fixed frequency.I would like to take the frequency command from PLC through profibus DP. For this i set up the parameters as in attachment. Status words(P2051.0-P2051.5) are coming fine. Motor Start command is from DI0/722.0. Speed Set-point command is from PLC via profibus address PQW354(only Transmitting value from PLC). So when i start the motor, its getting started taking current(100-200A), but doesn't rotate(no speed ref r2050.1(PZD2) = 0). My parameter settings are OK?? Do I need set/check any other parameter???
AttachmentG120_S7-300.docx (172 Downloads) |
Follow us on