5/16/2013 11:30 AM | |
Joined: 10/11/2006 Last visit: 3/13/2025 Posts: 5997 Rating:
|
Hello, The Sinamics G120 contains the possibility to connect the integrated digital inputs to the drivecontrols like OFF1 and so via Free Bico connection. For a fast commissioning you can use one of the available input marcos with parameter p15 to connect several inputs to drive control inputs. Maybe you can use the informations in the following documents: http://support.automation.siemens.com/WW/view/de/68670247/0/en http://support.automation.siemens.com/WW/view/de/71762451/0/en |
With best regards, |
|
Follow us on