Industry Online Support
Technical Forum
4/10/2013 1:22 PM | |
Posts: 7 Rating: (0) |
Hello, I would like to ask if I can reach safety Performance level=d (acc.EN13849-1) with driver Sinamics S120? HW configuration is: CU320 + SMC20 encoder module + motor encoder Lenord Bauer Minicoder GEL244. Encoder supplier specified in datasheet that encoder is usefull for safety functions (Output signal 1 Vpp with high signal quality (sin/cos)) but I would like to be sure. I would like to use SS1+SLS function with the drive. Thank you AttachmentEncoder_GEL244_e.pdf (74 Downloads) |
Follow us on