2/6/2007 11:26 AM | |
Posts: 4 Rating:
|
Hi, I need to use on fly homing function but I could not find a good document about this topic that explains F1, F2 ext.. And I want toknowapplications that we can use this homing type. Thanks for your helps... |
2/14/2007 11:10 AM | |
Joined: 10/11/2006 Last visit: 3/13/2025 Posts: 5996 Rating:
|
Hello, I think you mean the inner and outer window. So if the difference between reference setpoint and measured value is less than F1 or higher than F2, there is no correction (there is no window function if the reference point is not set). Please have a look at the attached document. Best Regards TechTeam AttachmentSINAMICS_S120_Drive_Functions_Function Manual_0306_eng.pdf (978 Downloads) |
With best regards, |
|
Follow us on