Industry Online Support
Technical Forum
11/3/2008 8:58 AM | |
Posts: 1 Rating: (0) |
Hello, Iwould like to knowabout the pre charging circuit. In case of MASTERDRIVE, If inverters are to powered-up and down in operation, then a pre-charging circuit for the DC link capacitors of the inverter must be provided.
(Refer to the Catalog DA65.10 6/48 pages) In case of SINAMICS S120, canI use the pre charging circuit like as MASTERDRIVE If motor modules are to powered-up and down in operation? AttachmentDC link components.pdf (536 Downloads) |
11/14/2008 10:12 AM | |
Joined: 10/5/2005 Last visit: 6/15/2023 Posts: 5 Rating: (0) |
Are you using the Sinamics S120 in combination with masterdrives? |
Last edited by: PD at: 11/14/2008 10:16 AM |
|
Follow us on