4/12/2022 2:12 PM | |
Joined: 2/15/2021 Last visit: 4/14/2022 Posts: 14 Rating:
|
Hi, I have a project that have developed over time. Its a home made hot tub that I have outside. It has a circulation pump, a heater and a pump to drain water from a pump well. All is running good now for many years. The next think i´m doing at the moment is to build a motorized cover. I have a 3-phase motor with gearbox, a Sinamics V20 frequence converter and two limit switches to control the cover. Start/Stop/Reverse is controlled by the DIs at the V20 and the speed is controlled with a potentiometer connected to the AI on the V20. I want to Open/Close the cover with the same button (1 physical button OR 1 soft button on the webpage) The solution I have in the Logo! is something I just came up with from testing in the simulation mode. But my thought is that there must be a simpler/more clever way to program this? Any tips or tricks for the program is appreciated. I always want to learn more :) AttachmentPoolstyrning_V2.3_inkl motor.zip (566 Downloads) |
Last edited by: mlindeloef at: 04/12/2022 14:13:51 |
|
4/12/2022 2:21 PM | |
Joined: 12/18/2014 Last visit: 7/28/2024 Posts: 33426 Rating:
|
The limit switches has NO contacts? |
4/12/2022 2:37 PM | |
Joined: 2/15/2021 Last visit: 4/14/2022 Posts: 14 Rating:
|
Yes they are. |
Follow us on