2/18/2019 6:07 PM | |
Joined: 4/28/2015 Last visit: 6/22/2021 Posts: 1 Rating: (0) |
Is it possible to use the SINAMICS V20 with a 1AC 120 V supply? If so, it a de-rating factor? |
2/18/2019 6:44 PM | |
Joined: 3/27/2008 Last visit: 1/15/2025 Posts: 1157 Rating: (142) |
The V20 will not function with a 120Volt supply, it is designed for 230Volt single phase only. |
Tractor |
|
Follow us on