9/30/2017 7:08 PM | |
Joined: 3/13/2015 Last visit: 12/2/2023 Posts: 26 Rating:
|
Hello Everbody, I try to control Sinamix V90 through PROFINET. Firstly i used Telegram 3 and then Telegram 102. But I couldn’t solve my problem. My problem is that i couldn’t prevent the motor to stop without ramp. The link regarding this issue is below. I have attached the configuration which I made via TIA PORTAL and its driver parameters.(I use PLC S71511C-1 PN) Where is my mistake? Regards. https://drive.google.com/file/d/0B5yx_fcwKbXbbldEQzJPSll6ZnM/view?usp=sharing AttachmentCONFIGURATION_PICTURES.zip (307 Downloads) |
10/2/2017 11:21 AM | |
Joined: 10/11/2006 Last visit: 6/27/2024 Posts: 5869 Rating:
|
Hello, to stop without ramp is not possible, only in case of OFF_2 - (coast stop). Therefore you have motion commands to reach a fix end position. 3.4 Positioning axis technology object 11.1.5 MC_MoveAbsolute V3 https://support.industry.siemens.com/cs/ww/en/view/109739589 Telegram for V90 is normally -Tel. 105. Example: https://support.industry.siemens.com/cs/ww/en/view/109739053 Manual: https://support.industry.siemens.com/cs/ww/en/view/109739497 |
With best regards, |
|
This contribution was helpful to
1 thankful Users |
10/5/2017 12:06 AM | |
Joined: 3/13/2015 Last visit: 12/2/2023 Posts: 26 Rating:
|
Thank you so much for your help |
10/11/2017 1:03 PM | |
Joined: 3/13/2015 Last visit: 12/2/2023 Posts: 26 Rating:
|
DearChristophD , Thank you very much for your kind help and for your useful information . Now my system operates successfully but except some failure. I kindly request you again to help me to correct them. 1)After I made “HOME” , I send servo to the position and then to the “zero” position back with the same speed . In this case there is no problem. But when transmission speed and turn back zero position speed are different, it causes deviation in beginning position. What is the reason of this case and how can I solve it? 2)Shortly after I operate the system, I take the failure with code: F1912. I have looked at the manual to solve this problem but I couldn’t. I’m sure that the reason why my system doesn’t operate stable is because of me. Since Siemens serves high precision in every system that require high speed and sensibility. Expecially I’m a big fan of Simotion Scount System and one of my biggest dreams is to set up a simotion scount system in the future. :D Thank you in advance. Best Regards. |
Last edited by: FAKSARAY at: 10/11/2017 1:16:35 PM |
|
10/11/2017 2:01 PM | |
Joined: 10/11/2006 Last visit: 6/27/2024 Posts: 5869 Rating:
|
Hello , please find attached information for Failor F1912 (source: SIMOTION Help-System). You have to check your clock rate (please check Execution-system) AttachmentF01912.pdf (356 Downloads) |
With best regards, |
|
This contribution was helpful to
1 thankful Users |
Follow us on