4/17/2018 12:08 AM | |
Joined: 4/2/2016 Last visit: 7/13/2022 Posts: 413 Rating: (6) |
I have a positioning system based on S7-1200 and Sinamics V90 + 1FL6061-1AC61-0AB1, two axes, control - Pulse / Direction Interface. similarly as in the example SINAMICS V: Controlled Positioning of a V90 with S7‑1200 via the Pulse/Direction Interface, with HMI (Set 7) https://support.industry.siemens.com/cs/ww/en/view/77467940 for control Pulse / Direction Interface I use 2 fast digital output (for each axis), SB 1222 DC 200 kHz 6ES7222-1BD30-0XB0. the example does not use position feedback, but I would like to use signals from the motor encoder, Sinamics V90 has an encoder output (TTL 5V), 6 outputs (A+,A-; B+,B-; Z+,Z-), And I would like to read it, S7-1200 have High-Speed Counters (HSC) x6 pcs., to each HSC can connect 3 digital inputs (eg., A+, B+, Z+), for two axes I need 2xHSC (6 digital inputs), the problem is that encoder output from Sinamics V90 TTL (5V DC), and HSC S7-1200 HTL 24V DC, we have different voltages, of course I could use an additional card 5V DC (eg. SB 1223 DC/DC 200 kHz 6ES7223-3AD30-0XB0), but I'm already using SB for fast digital output SB 1222 DC 200 kHz. What can you advise me? What kind of equipment (converter TTL/HTL) required? |
Last edited by: Jen_Moderator at: 4/17/2018 9:16:47 AMOptimized link. |
|
4/17/2018 2:23 PM | |
Joined: 4/28/2015 Last visit: 9/4/2024 Posts: 394 Rating: (55)
|
Hello, I think, the two possibilities for you are:
For doing this, maybe have a look at the following application example: https://support.industry.siemens.com/cs/ww/en/view/109749356 |
4/18/2018 7:51 PM | |
Joined: 4/2/2016 Last visit: 7/13/2022 Posts: 413 Rating: (6) |
how do you think I could use a EMB-Signal splitting http://www.bbn.com.tw/pdf/EMB.pdf converter TTL->HTL... |
Last edited by: _oleksandr_ at: 4/18/2018 8:26:45 PM |
|
4/24/2018 8:39 AM | |
Joined: 4/28/2015 Last visit: 9/4/2024 Posts: 394 Rating: (55)
|
Hello, please make a posting with your experience with these converters... |
Follow us on