10/9/2017 11:12 AM | |
Joined: 5/20/2014 Last visit: 9/26/2022 Posts: 57 Rating:
|
This depends if you encoder is incremental or absolute. If incremental use MC_Home mode: 3 and set active homing to 'Zero mark via PROFIdrive telegram and reference cam' if your using digital input to mark the home position - keep in mind that it will look for encoder zero mark after reaching the digital input, if that's not suitable for your application then select: 'Zero mark via digital input' If absolute the use MC_Home mode: 7. This will store axis CURRENT position as Home when triggered. Please refer to TIA Help to get more info on MC_Home. For further details on the types of homing (configured in TO) look at this link, point No 9.: http://tiaportalhowto.com/en/blog/how-to-configure-technology-object-positioning-axis/
|
tiaportalhowto.com -> TIA Portal Tips, Tutorials, Videos, and more... |
|
Follow us on