3/26/2018 8:24 AM | |
Joined: 4/2/2016 Last visit: 7/13/2022 Posts: 413 Rating: (6) |
at one point in time can only move one axis Y or Z, X-axis operates independently of the hydraulics (from one endswith to the other), The program should be both similar precision surface grinder https://www.youtube.com/watch?v=zcStwk34zkM&t=185s |
Last edited by: _oleksandr_ at: 3/26/2018 8:25:16 AMLast edited by: _oleksandr_ at: 3/26/2018 8:27:12 AMLast edited by: _oleksandr_ at: 3/26/2018 8:27:35 AMLast edited by: Jen_Moderator at: 3/26/2018 9:29:59 AMInserted video. |
|
3/27/2018 10:29 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (877) |
Hello, V90 is not designed to handle continuous motion control task. |
4/17/2018 9:01 AM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating: (172) |
New question published by _oleksandr_ is split to a separate thread with the subject Encoder output from Sinamics V90 TTL (5V DC) and HSC S7-1200 HTL 24V DC have different voltages. Best regards |
Follow us on