7/11/2016 5:57 PM | |
Joined: 1/21/2013 Last visit: 6/6/2024 Posts: 4620 Rating: (705) |
Hello to all, I have a hydraulic pump with a normal three-phase motor, I should control the pressure, now is 50 Hz 80 Bar, I should always control it in less i.e.always less than 50 Hz, for example, 20 Hz and 33 Hz, what do you do recommend how to drive? I navigated a bit and I saw Sinamics V20 which should be standard but has no Profibus interface, I need this interface, and now what do you recommend? Sinamics G120? But I don't have retroaction on the motor, it is equally possible? Excuse me but I have no experience here. SINAMICS Servo Pump - Drive Technologies - Siemens There is already a de facto control in the drive for these applications? Thank you Greetings |
7/16/2016 9:09 PM | |
Joined: 1/21/2013 Last visit: 6/6/2024 Posts: 4620 Rating: (705) |
Thanks friends , when I will have some time I'll watch the parameters , if I need ,I trouble you again
|
Follow us on