Industry Online Support
Technical Forum
5/16/2011 6:12 PM | |
Posts: 32 Rating: (0) |
Hello, I have a question about if is posible to use the TIM 3V-IE DNP3 like a Ethernet CP for to communicate a S7-300 with a PAC3200 by MODBUS TCP and in the same ethernet port send DNP3 data. I had communicated a S7-300 with a PAC3200 by MODBUS TCP using a CP343-1 Lean and in the same port communicate with Wincc SCADA by TCP/IP, but I didn't have working with SINAUT TIM 3V-IE DNP3. AttachmentArquitectura SINAUT DNP3.pdf (64 Downloads) |
Follow us on