3/5/2010 3:02 PM | |
Joined: 3/14/2008 Last visit: 11/19/2024 Posts: 2134 Rating: (955) |
Well, If you can take a look.. the MLFB is: 6GK7342 5DA00 0XE0. I'm using it as a intelligent slave, sendinga maximum of 32 bytes to master andrecieving also. The other 2 CPU's which have an integrated DP, I don't have any problems with? There are also on the same Profibus DP |
If I could help you, you can use the RATE button. Thank you. |
|
3/6/2010 5:33 PM | |
Joined: 3/14/2008 Last visit: 11/19/2024 Posts: 2134 Rating: (955) |
Hello Hulzhex, I didn't see your post! In the time I was posting, you posted also.... Anyway, I posted this question to clear up some confusion, but the opposite occurred. Thx CbO So in conclusion for me and other readers: - CP443-5 Basic -- not sure it can be used again (as we don't really needed because this module wasused for the interface to SCADA on Profibus and now it's on IE. ) - CP443-5 Extended --is released for PCS7 7.1 - CP342-5 -- is connected as I-slave toProfibus master and used to read out important data from S7300 to S7400 Thx for the replies! |
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on