2/24/2010 4:04 PM | |
Posts: 40 Rating: (1) |
Hy. i just come back from the machine. I did change p840 in starter to r722.0 and the number there is now correct (as you said 47318016). I'm attaching some pictures to give you more informations about my problem. Could be the problem maybe the starting procedure? 24V first to X24, than to X21 and then 400V to ALM (over Q0.0 like it says in sbr_33). AttachmentPictures.zip (437 Downloads) |
Last edited by: taubek at: 2/24/2010 4:10 PM |
|
2/24/2010 4:07 PM | |
Posts: 40 Rating: (1) |
adding some more pictures, hope they help
AttachmentPictures2.zip (380 Downloads) |
Follow us on