10/31/2016 10:02 PM | |
Joined: 5/18/2015 Last visit: 5/8/2024 Posts: 98 Rating: (1) |
Hello I have a DMG cnc machine (model : DMU 50 eco) This machine configuration by Sinumerik 810 power line I start up this machine by initial backup & now I have 2 alarm (attached picture). Please help me to solve this problem. Thanks a lot. ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 11/3/2016 12:41:14 PMNew subject after splitting SKAZEMCNC |
|
11/2/2016 8:17 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (877) |
Hello e_skazem, You should have created a new post for this problem by which you could have received the solution from other forum members much earlier. However, I would request Moderator to split this post & create new post. Now to your problem, alarm 14152 - Is related to tool carrier invalid orientation, error code - not displayed in your case & alarm 14710 - Is error in initialization sequence in function, which is also related to tool change error mode. Are these alarms displayed during part program? If yes, please check the part program. Have you recently modified or re-loaded machine data? If yes, please check if the correct data is loaded.
HTH. |
Follow us on