7/27/2021 11:16 PM | |
Posts: 22 Rating: (0) |
thank you! I will keep your advice in mind. Regards, FLEX |
7/28/2021 5:32 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (875)
|
Hello Flex, After going thru all your posts, I suggest you to follow below steps. 1. GHOST image back up which you mentioned, is it of OK HDD? i,e. is it of correct working HDD back up? Please check. 2. If yes, you simply need to restore on spare HDD, connect to your MMC & system should work. 3. If no, you need to get HDD compatible to your MMC, i.e. preloaded Siemens software, connect it to MMC & install on machine. With Simatic Manager Step7 v 5.4, go on line. You need to check your PG/PC hardware. If you have Siemens PG with MPI CP, port & MPI cable you can connect it to X120 port i.e. service port. If you don't have Siemens PG, with PC you need MPI adaptor with RS232 or USB interface (please note, RS 232 or USB interface is required for PC connection & not to NCU) You need to procure 6GK1571-1AA00 MPI adaptor from Siemens After going online, you need to configure NCU, PLC address as mentioend in your earlier post. Check profibus cable, bus connectors & their switch positions. First & last profibus connector must be ON & others must be OFF. Switch on the power of system & clear NC/PLC & reload .arc files (files which you attached in earlier posts should work, provided that those are correct one). Please refer attached sheet for the same. After restoring arc files, your system should boot & communication should establish with out any alarm/fault. Please note, if you have .arc files stored on HDD, you can restore those from HDD itself, not neccessary to connect external storage device. Please check once your system boots & starts with out any alarm/fault. HTH AttachmentData_Loading_810D_840D[1].pdf (183 Downloads) |
7/28/2021 12:19 PM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (875)
|
Hello, Your NC seems to be quite old, as such I donot have correct documentation of it also HDD capacity is also very low. I guess HMI advance software also will not be of much useful in your case. I suggest to check 6FC5210-0DA20-0AA1 MMC which is successor for MMC102 which you purchased. Try for this MMC on siemens mall & search for this 6FC5210-0DA20-0AA1 MMC. HTH |
Last edited by: PISCEAN 2010 at: 07/28/2021 12:20:55 |
|
Follow us on