6/20/2023 4:23 PM | |
Joined: 10/11/2022 Last visit: 2/28/2024 Posts: 2 Rating:
|
We have a Hyundai HIT 30S with 840C control. IMG_01 show the control type as SINUMERIK 840-C T E and the NCK Software version as V04.09.50 97/12/10. The machine was without power for some time and the backup battery depleted. We replaced the battery, restarted the machine, but had several errors shown in IMG_02. The first error was 43-plc not ready. Details of the error are shown in IMG_04. The version and date for the ANW_PROG information are also blank as shown in IMG_05. I went through the general reset procedure, and restored the ANW_PROG from backup, but the error was not resolved. When doing the GEN RESET, there were 5 files listed under Start-up/Machine data/User data as shown in IMG_06. The S30S file would not load, but any of the other 4 would. AttachmentHIT 30S.zip (266 Downloads) |
6/21/2023 1:44 PM | |
Joined: 10/11/2022 Last visit: 2/28/2024 Posts: 2 Rating:
|
Thank you. I have contacted support via email. |
Follow us on