11/24/2023 6:22 AM | |
Joined: 10/18/2023 Last visit: 12/20/2023 Posts: 4 Rating: (0) |
I replace one NCU 710.3B PN, I use the CompactFlash Card old .When power is applied to the NCU 710.3 PN, all the LED indicators light up (orange), the digital LED is on 0 and 2, the led ready not flash and move green? NCU not boost ok ? help me how to fix? ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 11/24/2023 09:16:48New subject after splitting |
|
11/25/2023 11:58 AM | |
Joined: 1/24/2021 Last visit: 5/5/2024 Posts: 187 Rating: (21) |
Your "mode selector" switches are in "not working" position. Read the attached manual to make general reset of NCK and PLC, then leave switches in "0".
AttachmentReset NC and PLC.pdf (560 Downloads) |
People are divided into those who do Backup and those who will do it. |
|
Follow us on