8/30/2022 2:21 AM | |
Joined: 3/22/2022 Last visit: 11/1/2022 Posts: 69 Rating: (1) |
Another machine with alarm no PLC STOP |
8/30/2022 6:49 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (873)
|
Hello, I suggest you to refer below manuals which will help you to put machine back into operation. SINUMERIK 810M, GA1, Operating and Programming SINUMERIK 810M, GA2, Operating and Programming SINUMERIK 810M/820M/850M/880M, Shopfloor UMS, Function Blocks, Planning Guide SINUMERIK 810M/820M SINUMERIK 850M/880M Shopfloor UMS Function Blocks SINUMERIK 810M/820M/850M/880M, Shopfloor UMS, Measuring with Operator in JOG Mode SINUMERIK 810M/820M/850M/880M, Shopfloor UMS, Menu Trees, Planning Guide SINUMERIK 810M/820M/850M/880M, Shopfloor UMS, Drilling & Milling Cycles, Programming Guide SINUMERIK 810M/820M/850M/880M, Shopfloor UMS, Contour Calculation, Programming Guide SINUMERIK 810M/820M/850M/880M, Shopfloor UMS, Technology Calculation |
8/31/2022 3:10 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (873)
|
Hello M. Shafay, I read your all related topic of this system. If I were you, I would had recommended the machine owner below points. 1. Just go for replacement/retrofitting of 810M/820M system by an equivalent system, instead of trying to put this system operational. 2. Since its quite old system, system software support along with necessary peripheral accessories like, PG/PC back up software, versions, HMI etc. etc. is limited. 3. System, drives. motor spares are obsolete i.e. service support not available. 4. Technical expertise of this system is very limited & will be helpless in case of unavailability of hardware or software support. Even though you succeed to start the system, machine productive efficiency will be very low. Sooner or later user has to go for retrofitting. As such the sooner you get it retrofitted the more beneficiary it would be. Hope this helps. |
This contribution was helpful to1 thankful Users |
8/31/2022 10:57 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (873)
|
Yes I understand. Good luck, all the best. |
8/31/2022 11:10 AM | |
Joined: 8/21/2014 Last visit: 5/24/2024 Posts: 959 Rating: (13) |
Closed cause question posted twice. The second thread with the subject"SINUMERIK 810M machine lost parameter, how to recover"is published within the conferenceSINUMERIK CNC automation systems Best regards, |
My Forum is the place to personalize your profile, |
|
Follow us on