5/4/2023 7:18 PM | |
Joined: 6/1/2022 Last visit: 8/22/2023 Posts: 5 Rating: (0) |
Hello, I'm trying to commision a sinumerik one system (NCU 1740, ver. 6.15). I've gotten to the point of trying to download the PLC program. I can compile with no errors on the software or hardware. When I try to actually set the PLC to RUN, it immediately runs into an error. SINUMERIK message: DB access error: DB1000 Explanation: An error occurred during access to the data blocks, the data block cannot be used. See alarm: 404007 Then: Temporary CPU error: User programmed STOP request in FB 25003 affecting OB 1 execution I have not been able to find any reference to alarm 404007, or errors related to FB25003(LBP_InternalProc7) or DB1000(LBP_CtrlEnergy) AttachmentDiagnostics.txt (270 Downloads) |
5/9/2023 7:25 AM | |
Joined: 7/12/2021 Last visit: 1/15/2024 Posts: 26 Rating: (3) |
Is the toolbox in your project actually and also loaded to the PLC? |
5/9/2023 1:13 PM | |
Joined: 6/1/2022 Last visit: 8/22/2023 Posts: 5 Rating: (0) |
Yes it is |
Follow us on