7/9/2024 2:06 PM | |
Joined: 4/5/2023 Last visit: 7/9/2024 Posts: 1 Rating: (0) |
Hey everyone - I've taken an archive from a SINUMERIK 840D SL running Operate 4.8 SP7 HF1, and every time I've tried to launch it, I've received an error code. I've solved several now by taken files directly from the 840D and replacing them on my SINUTRAIN PC, but I've reached the point of "this cant be right". The machine that was created by the import process states that its running with the "840D sl 4.8 SP4" profile/template - is this the issue? I've tried looking for a SINUTRAIN version that can create 4.8 SP7 templates, but haven't found anything. Currently, when I run the machine, this is the error in run_hmi.log is as follows:
AttachmentCrash Log.txt (18 Downloads) |
Last edited by: Wit_Moderator at: 07/10/2024 12:38:03Crash Log attached as txt-file |
|
Follow us on