4/12/2024 9:43 AM | |
Joined: 10/9/2007 Last visit: 7/11/2024 Posts: 1246 Rating:
|
Hi you need an additional packet with IEC61850/MMS driver for this. SICAM SCC is one option, which offers several templates for the control of typical substation primary equipment, such as circuit-breaker and disconnectors. It also offers other functionalities, such as topological coloring, which colors the single line diagram based on voltage presence and swichgear positions. It imports data from the SCD to Tag Management, Tag Logging and Alarm Logging. More information SICAM SCC - SiePortal - Siemens RC-DE |
Energy Automation products: Sicam, Siprotec, Digsi |
|
Follow us on