8/21/2013 12:50 PM | |
Joined: 11/8/2011 Last visit: 7/2/2024 Posts: 387 Rating:
|
find diagnostic screen shot |
8/21/2013 12:51 PM | |
Joined: 11/8/2011 Last visit: 7/2/2024 Posts: 387 Rating:
|
Hardware config screenshot |
8/21/2013 4:01 PM | |
Joined: 9/27/2006 Last visit: 8/14/2024 Posts: 12277 Rating:
|
Hello Saggy; Look at the attachment, taken from the following manual (part of the documentation ^proposed earlier): http://www.energy.siemens.com/ecc_pool/SIPROTEC4/f215125d-6567-4bf0-9362-f6e6efdfab7a/pdp_7sj6263_e.pdf It reflects Mapping 3.1, 100 bytes IN, 9 bytes OUT. Try reproducing this mapping exactly in your module selection in HWConfig: continuous addresses in byte format, I addresses first, Q addresses at the end, and no consistent values selection. Tell us if the configuration is more acceptable to the CPU this way. Hope this helps, Dniel Chartier |
This contribution was helpful to
2 thankful Users |
8/22/2013 8:21 AM | |
Joined: 11/8/2011 Last visit: 7/2/2024 Posts: 387 Rating:
|
Hi dchartier , Thanks again for the reply I have configured in HW configuration IN 100 byte and 9byte OUT in the sequence addresses first IN and then OUT but still i have the same error stating CONFIG FAULT Please guide in th DIGSI software i have selected 3-1 mapping it will select the mapping data standard format or i need to configure manually Thanks in Advance |
Follow us on