2/4/2012 3:09 PM | |
Joined: 11/21/2007 Last visit: 9/25/2024 Posts: 2325 Rating: (308) |
Hello All We need to connect SIPROTEC Relays on Profibus to a S7-300R ( CPU 315-2 PN/DPs with SoftWare Redundancy. As has been discussed many times in this Forum, SWR systems do not support Y-Link Modules ( Though no clear reason has ever been given ), unless there are any new developments that I may not be aware of. Therefore we plan toconnect the relays with the Two CPUs through RS485 repeaters Similar to the solutionprovided in FAQ below for connecting HMIs toS7-400H Systems. : http://support.automation.siemens.com/WW/view/en/23842653 Now Unlike normal Profibus Slaves ( Drives , ET200S etc ) the SIPROTEK Relays are not "Controlled Slaves" of the S7 system in the sense that the S7 system Mostly Reads data cyclically from the relays, besides occasionally issuing some commands. The Worst possible Scenario that we can imagine is that the communication from CPU to relays would be interrupted during the period of changeover of the CPUs and switching of the Repeaters.and establishment of Profibus connection from the new Master CPU to the Relays. If our application permits this, then are there any other problems that might arise in implementing this solution. If anyone can suggest a better solution ( Other than going in for S7-400H - Our Budget does not permit that ), that is most welcome. Thanks Navnag |
There is no such thing as the last bug in a program |
|
This contribution was helpful to1 thankful Users |
2/15/2012 11:47 AM | |
Joined: 10/7/2005 Last visit: 10/4/2024 Posts: 3024 Rating: (1054)
|
Hello Navnag I only know about the devices below and haven't used either of them yet, so I can't say how they perform in real life, but you may be interest in them nonethelss as a possible solution foryour particular "challenge": COMSOFT's PRS ABB's RLM01 I hope this helps and good luck with your project. |
Cheers |
|
This contribution was helpful to2 thankful Users |
4/10/2013 2:11 PM | |
Posts: 153 Rating: (2) |
I have tested COMSOFT's PRS with swr redundent system, these were the results: - during the switch over b/w cpus , we are lossing communication with the n/w attached with PRS. - I remember , my stand by CPU is always showing BF i found not feasible , so i drop the idea... |
This contribution was helpful to3 thankful Users |
Follow us on