12/7/2018 6:23 PM | |
Joined: 8/9/2016 Last visit: 8/4/2024 Posts: 70 Rating:
|
Hi, I've got an LR250 transmitter and RD100 display which are to be connected with 24DC power supply, based on loop back power (HART protocol compliant) A slight confusion on the wiring diagram which are attached. The first one is from SIEMENS web based documentation and show the -ve of the transmiiter connected with the +ve of RD100. However, te second diagram which came along the instrument documentation show the -ve of transmitter connected to the -ve of RD100. Logically, the conncetions should be like this. From +ve of Power supply to the +ve of transmitter, then from -ve of transmitter to the +ve of RD100, and finally from -ve of RD100 to the -ve of P.Supply. Please suggest so that the instruments work perfectly. Attachmentdig.pdf (315 Downloads) |
12/7/2018 9:58 PM | |
Joined: 8/9/2016 Last visit: 8/4/2024 Posts: 70 Rating:
|
Thank You for the feedback danw. I'll post after testing |
12/18/2018 3:30 PM | |
Joined: 8/9/2016 Last visit: 8/4/2024 Posts: 70 Rating:
|
the Diagnositc Status of the AI cards is also attached |
Follow us on