6/10/2016 11:24 AM | |
Joined: 5/23/2016 Last visit: 11/15/2023 Posts: 63 Rating:
|
I've come by these getting started packages: Getting Started Packages Siwarex CS TIA V13 These will not work when using the S7-1500 because of a a few knowhow protection blocks when changing from PLC.
I also tried to migrate the entire project to the S7-1500, this solved a few errors. Except, it won't migrate the knowhow protected blocks. Would there be a way around this, or is it just not possible to use the Siwarex CS with a S7-1500? |
Last edited by: Dominiques at: 6/10/2016 12:40:09 PMLast edited by: Dominiques at: 6/10/2016 12:40:43 PMBest Regards, |
|
6/14/2016 8:18 AM | |
Joined: 5/23/2016 Last visit: 11/15/2023 Posts: 63 Rating:
|
After quite some time doing research, i've found that it is possible to use the SIWAREX CS with the S7-1500. Contact, hotline.siwarex@siemens.com they will provide the information and sotftware to get started. There isn't a download page for this, so you'll find the software in the attachment and a document with more information in my next post! AttachmentS7_1500_SIWAREX CS_TIA_V13.zip (344 Downloads) |
Best Regards, |
|
6/14/2016 8:18 AM | |
Joined: 5/23/2016 Last visit: 11/15/2023 Posts: 63 Rating:
|
Here's the document! AttachmentFAQ_SIWAREX_CS_S7_1500_eng.pdf (447 Downloads) |
Best Regards, |
|
This contribution was helpful to
1 thankful Users |
10/30/2017 1:09 AM | |
Joined: 3/11/2015 Last visit: 11/30/2023 Posts: 1 Rating:
|
Thank you so much! This helped me a great deal. |
Follow us on