12/6/2019 3:22 PM | |
Joined: 9/27/2006 Last visit: 12/4/2023 Posts: 12187 Rating:
|
Hello SP: You can insert a Siwarex FTA as part of the ET 200M station (IM 153-2 Profibus head module) that you setup on tyour 3rd-party master. See ths FAQ on a Siwarex FTA with a S7-400 master (the Siwarex unit is a S7-300 module, so you have tio insert an IM 153-2 in the S7-400 Profibus configuration to set it up): How can the Siwarex U, FTA, FTC be integrated in S7-400? https://support.industry.siemens.com/cs/us/en/view/10182429 Confirmation in this sales document: https://www.automation.siemens.com/salesmaterial-as/brochure/en/brochure_simatic-et200_en.pdf Here are the gsd files for different model numbers of IM 153-2, choose the one that corresponds to your IM 153-2 unit and insert it in your master's Profibus configureation: PROFIBUS GSD files : ET 200M https://support.industry.siemens.com/cs/us/en/view/113498 Once the IM 153-2 is integrated as a slave on the Profibus network, open the modules catalog to select I/O modules and function modules, such as the Siwarex FTA. Hope this helps, Daniel Chartier |
12/9/2019 12:29 PM | |
Posts: 3 Rating:
|
Clear, thank you very much! |
Follow us on