4/7/2009 9:16 AM | |
Joined: 5/28/2008 Last visit: 7/15/2024 Posts: 1343 Rating: (141) |
Hi, have you seen this? [url]http://support.automation.siemens.com/WW/view/en/30347016[/url] |
4/7/2009 10:21 AM | |
Posts: 3 Rating: (0) |
Thanks but I'm stillnot to sure how to enter the zero point and the calibration weight 1. |
4/7/2009 4:31 PM | |
Joined: 1/4/2007 Last visit: 7/11/2024 Posts: 1134 Rating: (175) |
Hello ttevol, Into the internet you can find a Getting Started example project, with a Step7 program and the TP177micro panel. The link is: http://support.automation.siemens.com/WW/view/en/22605342 Into the manual of the Siwarex MS module,chapter 8.10.2 (Figure 8-17), you can see, how to do a calibration with the TP177micro panel.You can download the manual with the following link: http://support.automation.siemens.com/WW/view/en/22600601 Best regards Siwarexi |
5/11/2009 1:36 PM | |
Joined: 1/4/2007 Last visit: 7/11/2024 Posts: 1134 Rating: (175)
|
Dear DesertDog, the latest documentation is not “very vague using the 26 original commands”. As you can see into the chapter 6.2 all commands are described. Also into the chapter 8.9 the command-executing via Step7 is described step by step. You can download the current manual with the following link: http://support.automation.siemens.com/WW/view/en/22600601 If you get the Error #1 (Not Supported on this module), your Siwarex MS module has not the current Firmware V1.3. Therefor, you can read the words „E-Stand 03“ on the housing of the Siwarex MS module. What „E-Stand“ has your Siwarex MS module? I look forward to hearing from you. Best regards Siwarexi |
Last edited by: Siwarexi at: 5/11/2009 1:39 PM |
|
Follow us on