12/1/2024 3:24 AM | |
Joined: 1/16/2012 Last visit: 12/5/2024 Posts: 116 Rating: (2) |
Dear Experts, I have two similar machines equipped with loadcell/SIWAREX. I have received all the data from both SIWAREX modules through SIWATOOL V7. After receiving the data, I saved and exported both backups to CSV files. When comparing them one indicates the number of load cells as 1, while the other shows the number of load cells as 3. It is referring to DR10-8, however, I can't see this parameter in SIWATOOL. Could you please guide me on where SIWAREX is obtaining this setting or parameter? Thank you. I have attached both CSV files. Best Regards, Tech Ahmed AttachmentParameter.zip (26 Downloads) |
12/2/2024 7:52 AM | |
Joined: 1/4/2007 Last visit: 1/3/2025 Posts: 1170 Rating: (175)
|
Hello Tech Ahmed, What Siwarex module do you have (WP231, WP251, …)? Best regards Siwarexi
|
12/5/2024 7:50 AM | |
Joined: 1/16/2012 Last visit: 12/5/2024 Posts: 116 Rating: (2) |
Hi Siwarexi, It is WP231. Thanks. |
12/5/2024 12:17 PM | |
Joined: 1/4/2007 Last visit: 1/3/2025 Posts: 1170 Rating: (175)
|
Hello Tech Ahmed, Can you post two Siwatool files from your two WP231 modules, please. Attached a pdf-file how to create a Siwatool file. I would like to take a look into the Siwatool files. Best regards Siwarexi
Attachmentcreate_a_SIWATOOL-file.pdf (18 Downloads) |
Follow us on