8/7/2010 9:04 AM | |
Posts: 8 Rating: (0) |
Dear All, Is there any difference between the OldSIWAREXU (MLFB7MH4950 2AA01) & New SIWAREX U(MLFB7MH4601-1BA01).
|
Last edited by: avi6630 at: 8/7/2010 9:13 AM |
|
8/7/2010 2:40 PM | |
Joined: 9/27/2006 Last visit: 1/22/2025 Posts: 12330 Rating: (2702) |
Hello Avi; Here is what you will find on the A&D Mall on 6these 2 units: 7MH4950-2AA01 SIWAREX U WEIGHING ELECTRONICS (TWO-CHANNEL VERSION) * FOR CONNNECTING TWO SCALES * FOR SIMATIC S7-300 AND ET200M * RS232 INTERFACE FOR CONNECT. OF A PC * TTY INTERFACE FOR REMOTE DISPLAY CONNECTION WITH BUS CONNECTOR The Product 7MH4601-1BA01 is outdated. The successor product is shown aboveAs Ammy said, dufferent versions of the same product. |
8/10/2010 6:12 AM | |
Posts: 8 Rating: (0) |
Thanks for the reply.. but is there anydifference inexcitation voltage provided by Siwarex module to the Load cell . .
|
8/10/2010 2:50 PM | |
Posts: 8 Rating: (0) |
is it like that the new one has a excitation voltage of 6Vdc and the old one had 10 Vdc. |
8/11/2010 8:27 AM | |
Joined: 4/24/2006 Last visit: 1/22/2025 Posts: 8808 Rating: (1173) |
I think so. Best regards, Wizard |
10/26/2016 12:35 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4766 Rating: (122) |
New question published by AutoGen_558785 is split to a separate thread with the subject SIWAREX U interface with Computer with out any S7-300 cpu. Best regards |
Follow us on