8/17/2016 7:05 AM | |
Joined: 5/6/2010 Last visit: 8/5/2024 Posts: 1975 Rating: (275) |
Hello Bertus@NBL, you need the SIWATOOL for configuration the WP231, please look at this document: Hope it helps. |
8/26/2016 10:14 AM | |
Joined: 1/4/2007 Last visit: 8/9/2024 Posts: 1137 Rating: (175)
|
Hello Bertus@NBL, Unfortunately CaOd is not right. It’s not necessary to use the Siwatool software to configure the WP231 module. You can find an example project on the internet (file: “ready_for_use_modbus.zip”): With this example project you can connect a TP700 HMI-panel directly to the WP231 module and you configure the WP231 module via the TP700. If you change the IP-address of the WP231 module, you also have to change the partner-IP-address of the HMI-panel (= IP-address of the WP231 module) into the TIA Portal software.
|
This contribution was helpful to1 thankful Users |
8/29/2017 1:44 PM | |
Joined: 8/21/2014 Last visit: 8/12/2024 Posts: 1006 Rating: (13) |
New question published by msgsadek is split to a separate thread with the subject Can you guide me if i want to use KTP1200 BASIC instead of TP700 ??. Best regards |
My Forum is the place to personalize your profile, |
|
Follow us on