11/20/2017 9:32 AM | |
Joined: 1/4/2007 Last visit: 8/9/2024 Posts: 1137 Rating:
|
Hello bach2626, No matter which settings you are using for your USB/RS485 converter. The Siwatool software set the parameter settings correctly for the communication. I recommend you to use the USB/RS485 converter, which is mentioned into the manual of the WP321 module: USB-Nano-485 of the company CTI leancom http://www.cti-shop.com/RS485-Konverter/USB-Nano-485 ThisUSB/RS485 converter is working without any problems. Best regards Siwarexi |
This contribution was helpful to
1 thankful Users |
7/29/2020 1:29 PM | |
Joined: 1/4/2007 Last visit: 8/9/2024 Posts: 1137 Rating:
|
Sorry, I forgot to explain the hardware-connection of the USB-Nano-485 of the company CTI leancom in my post of 11/20/2017 9:32 AM: I wrote only: I recommend you to use the USB/RS485 converter, which is mentioned into the manual of the WP321 module: USB-Nano-485 of the company CTI leancom http://www.cti-shop.com/RS485-Konverter/USB-Nano-485 Here the hardware-connection. It's quite easy: The USB-Nano-485 of the company CTI leancom has to be connected by this way: - USB-NANO-485 (CTI), pin A => WP321 module, pin 13 (D+) of the base unit Best regards Siwarexi |
Follow us on