5/25/2021 9:25 AM | |
Joined: 1/4/2007 Last visit: 7/11/2024 Posts: 1134 Rating:
|
Hello adminals, 1. Can you send to me one photo, in which I can see the LEDs of the two Siwarex WP321 modules, please? 2. Can you download the Ready-for-Use project (the first Download-link) from this webside, please: https://support.industry.siemens.com/cs/ww/en/view/94109373 Use the Ready-for-Use project with the FB321 V4.4. Call only the first WP321 with this Ready-for-Use project: Is the fist WP321 running now? 3. I saw in your screenshot, that you are using the Multiplex-project: Did you follow the procedure how to use the Multiplex-project? There exist a pdf-file. In this pdf-file, the procedure is explained how to use the Multiplex-project. 4. Send to me your TIA Portal project, please. I would like to take a look into it. Maybe I find a mistake. (I don't need your visualisation, only the FB321 call in your S7-program and your Device configuration.) Best regards Siwarexi |
Follow us on