7/15/2014 11:30 AM | |
Posts: 23 Rating: (0) |
Hello, experts! We face a problem during project migration from PCS7 7.1 to PCS7 8.0 SP1. There are several SiwarexU 2ch modules 7MH4601-1BA01 in our project, and initially we use SiwarexU 7MH4683-3BA64 V42 library to integrate it to our project, and it works fine, even SIWA_U block connects to diagnostics (module drivers). But now we moves to PCS7 8.0 and I could not see Siwarex modules in HW config and it is goes to Read-Only mode. What opportunityes we have except replace modules to newer ones? According to Siemens documentation in attachements such modules is too old for PCS7 8.0, but probably we can still use it without channel drivers in worst case? AttachmentSiwarexU not supported.pdf (63 Downloads) |
7/15/2014 1:02 PM | |
Posts: 567 Rating: (106) |
Hi, you have to install the HSP to include the old hardware into the hardware profile. Then you will see the SIWAREX U in HWconfig! http://support.automation.siemens.com/WW/view/en/48549017 |
This contribution was helpful to1 thankful Users |
Follow us on