4/29/2019 8:54 AM | |
Joined: 1/4/2007 Last visit: 12/17/2024 Posts: 1166 Rating: (175)
|
Hello JBee, Follow the steps below, please: 1. Don’t install the software from a network-device, please. At first, copy the whole software to your local PC. 2. Please remove once again your "old" Siwatool V7 software into the operating system Windows: 1. the software "SIWATool V7" 2. the software "SIWATool Firmware All WP Devices"<- VERY IMPORTANT! 3. delete the following folders: "SIWATool V7" in the directory C:\Program Files (x86) “SIWATool V7“ in the directory C:\ProgramData (ProgramData is a hidden folder) *) “SIWATool7“ in the directory C:\Users\YourUserName\AppData\Local (AppData is a hidden folder) *) 4. Install the new software: Execute the file "SIWATool_V7_Setup.exe" with a mouse right click-->run as administrator. * How to show a hidden folder: https://support.microsoft.com/en-us/help/14201/windows-show-hidden-files Best regards Siwarexi |
This contribution was helpful to3 thankful Users |
12/8/2019 12:27 AM | |
Posts: 1 Rating: (0) |
This was very helpful for me also..thanks |
2/18/2023 3:59 PM | |
Joined: 6/10/2016 Last visit: 9/14/2024 Posts: 7 Rating: (0) |
Very helpful. Followed the steps as stipulated and its working now. |
Follow us on