Industry Online Support
Technical Forum
7/26/2011 10:38 AM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181) |
Hello, Descriptions about differences in Windows7 is there - http://en.wikipedia.org/wiki/Windows_7_editions My opinion is that as Sizer is released to work under Ultimate edition should works under Enterprise edition too. In order to make installation you should change the setup file of Sizer. Take it in mind that is possible after successully installation under Enterprise, Sizer might not work properly. Best regards, Hristo Mihalev |
7/27/2011 1:32 PM | |
Posts: 31 Rating: (0) |
How can I change the setup file to ignore the Operating System check. I have looked through many of the .INI files and this is not clear to me. |
Follow us on