10/18/2023 11:47 PM | |
Joined: 12/18/2014 Last visit: 7/26/2024 Posts: 33421 Rating:
|
Have you really a Master/Slave procedure? Or mean you Client/Server? |
10/19/2023 2:50 PM | |
Joined: 5/14/2020 Last visit: 7/11/2024 Posts: 12 Rating:
|
I have 2 PLC. 1 behaves like a Master, the other PLC is slave. |
10/20/2023 1:14 AM | |
Joined: 12/18/2014 Last visit: 7/26/2024 Posts: 33421 Rating:
|
First of all: Attached is a small network project that shows you the diagnostic query for the “Ethernet link error”. In addition, the generation of a life bit and its evaluation. A signal is generated in the client LOGO!, which changes state every second. The signal is sent to the server LOGO!. There it is asked whether it is either HIGH or LOW for longer than 1.5 seconds. If this is the case, communication is interrupted. At the same time, the received life bit is sent back unchanged to the client LOGO! and evaluated there. AttachmentCommunication_error.zip (337 Downloads) |
Last edited by: ixo65 at: 10/20/2023 01:15:05 |
|
Follow us on