Industry Online Support
Technical Forum
3/28/2011 7:38 PM | |
Posts: 52 Rating: (0) |
Hi All, In my project, am using MP277 & application is developed in WinCC Flexible 2007. I would like to use a stand alone machine ( with windows XP OS) as a sm@rtclientto access these HMIs. How to configure a stand alone machine as a sm@rtclient? Cheers, AB |
3/30/2011 9:04 AM | |
Joined: 4/29/2010 Last visit: 8/12/2024 Posts: 1557 Rating: (161)
|
Hello, if you don`t want to look from a flexible runtime to the panels you just need the Sm@rt Viewer in this case. You can find all needed information at the flexible getting started for options: http://support.automation.siemens.com/WW/view/en/18657078 best regards |
4/4/2011 12:56 PM | |
Posts: 52 Rating: (0) |
Hi Sandman... Thanks for sharing such an useful manual... Actually the PC machine which i will be using to monitor remote HMI through sm@rtclient, will not be having any WinCC Flexible S/W on it. I was told that siemens has an utility which only install sm@rtclient component on the machine. How can i get that utility/installable for sm@rtclient? Thanks, Anil |