3/1/2016 7:37 AM | |
Joined: 9/17/2015 Last visit: 6/13/2024 Posts: 137 Rating:
|
I have selected following hardware fr my project. I have a encoder with 250 PPR(pulse per revolution) From the hardware given below please tell me if I can connect my encoder to the input module or not. I have read few threads in forum but none is exactly related to my problem. CPU 319-3 PN/DP Input module - SM 321 - 16 DI - MLFB - 6ES7321-1BH02-0AA0 I hope this information is enough, if more information required feel free to ask. |
3/1/2016 12:47 PM | |
Joined: 9/16/2013 Last visit: 5/28/2024 Posts: 199 Rating:
|
100 rpm *250 ppr= 25000 pulses per minute 25000/60 = 417 pulses per second i think thats to fast for simatic s7-300. ---- You should connect your Encoder to your drive. Have a look at: https://support.industry.siemens.com/cs/de/en/view/78794884 (page 66) |
This contribution was helpful to
1 thankful Users |
3/2/2016 5:01 AM | |
Joined: 9/17/2015 Last visit: 6/13/2024 Posts: 137 Rating:
|
Can you suggest me any S7300 series CPU which has 2 DP 1 PN port and I can connect encoder input to it. |
Follow us on