6/2/2023 8:31 AM | |
Joined: 5/30/2022 Last visit: 11/29/2023 Posts: 440 Rating:
|
Hi BlocloT, WinCC Unified has no SNMP client inside, so it is not possible to connect to a SNMP server. So you have to write your own SNMP client, runs it on the Unified Server machine and exchanges the needed payload with WinCC Unified via RT ODK or OpenPipe. Further information can be found here: SIMATIC HMI WinCC Unified Open Pipe |
Last edited by: Hazard_7 at: 06/02/2023 08:34:32If this information really helps, you could use the Rate function. |
|
Follow us on