5/31/2019 7:22 AM | |
Joined: 9/21/2012 Last visit: 3/26/2023 Posts: 3659 Rating:
|
There should be no problem in changing an input to an other. |
5/31/2019 9:19 AM | |
Joined: 12/9/2010 Last visit: 10/8/2022 Posts: 623 Rating:
|
Hi ara12, Use the spare input & make connections. U can use rewire function to automatically replace old ip address with new address. See attachment. |
If you like the comment, rate it (right top) or thank it (left bottom). |
|
5/31/2019 11:25 PM | |
Posts: 11 Rating:
|
Thanks experts, i do, and will let you know the status. ars12 |
6/1/2019 12:58 AM | |
Posts: 11 Rating:
|
Dear Experts, I tried to rewire as you said but it show the error message, please see attached screenshot, Thanks, ara12 |
6/1/2019 2:44 PM | |
Joined: 12/9/2010 Last visit: 10/8/2022 Posts: 623 Rating:
|
Hi ara12, The project appears to be not consistent or not organized. Perform 'check block consistency'. |
If you like the comment, rate it (right top) or thank it (left bottom). |
|
6/4/2019 1:01 AM | |
Posts: 11 Rating:
|
Dear Sachin, I tried "check block consistency" but here also i faced problem, see attached pic1&2, is it possible that i goto specific FC and change the address only there, see pic03 As I20.3 is using only in FC20 at NW01 to I20.6(which is spare) save and download only changes? Thanks ara12 AttachmentPic.zip (61 Downloads) |
6/5/2019 2:40 AM | |
Posts: 11 Rating:
|
Thanks dear All, its done by changing the the address in FC only, Regards, ara12 |
Follow us on