11/2/2011 12:29 PM | |
Joined: 10/7/2005 Last visit: 5/15/2024 Posts: 3005 Rating: (1048)
|
Hello patel I'm afraid to say that my answers are possibly not the ones you want to have, but here they come anyhow: 1.) Q: "can i use the normal DIN RAIL & normal BUS connectors to connect my I/O modules on DIN RAIL"? A: No 2.) Q: "please give me any alternative which can be used instaed of active bus unit" A: There is no alternative, you must usetheactive bus modules See also Page 63 of the SIMATIC S7-300/S7-400 Software redundancy manualor THIS FAQ which state that: ET 200M stations must always be set up with active bus modules (6ES7195-7HB00-0XA0 or 6ES7195-7HC00-0XA0), even when the function "removing and inserting I/O modules in Run mode of the CPU" is not possible due to the design principle of S7-300 CPUs. |
Last edited by: fritz at: 11/2/2011 12:31 PMCheers |
|
Follow us on