4/30/2010 10:42 AM | |
Posts: 8 Rating: (0) |
Hello.I'm newbie in Siemens. Now, I have a question about software redundancy with S7-315-2DP. I configured hardware according to attachment. I want to know how to program software redundancy. (communication MPI) P.S. sorry about my English language. AttachmentNet Pro.pdf (402 Downloads) |
4/30/2010 4:10 PM | |
Joined: 7/2/2008 Last visit: 9/30/2024 Posts: 928 Rating: (308)
|
Hello nookamon, What you have to do is to read the software redundancy manual carefully before you start programming. In chapter 5, you will see that you should use blocks from XSEND_300 block package which can be found under SWR_LB library. You can also look at the example projects. Example projects and SWR_LIBcan be found when you install the runtime software. Best regards. H-H |
5/3/2010 5:24 AM | |
Posts: 8 Rating: (0) |
In example it used CP 342-5 but I don't wanna use it. I attached the hardware configuration for your information. AttachmentHardware configuration.zip (370 Downloads) |
5/3/2010 5:59 AM | |
Joined: 10/7/2005 Last visit: 10/15/2024 Posts: 3024 Rating: (1054)
|
Hello nookamon as H-Hsaid: "In chapter 5, you will see that you should use blocks from XSEND_300 block package" (if you want to use MPI for the link between the CPU's). Please note also Chapter 6.7 which states: "The two stations canbe linked via MPI, PROFIBUS or Industrial Ethernet. |
Last edited by: fritz at: 5/3/2010 6:02 AMCheers |
|
Follow us on